Fusion 7' touchscreen not initialized correctly on imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fusion 7' touchscreen not initialized correctly on imx6q

1,178件の閲覧回数
nxpsri
Contributor II

I'm seeing the following fusion-ts driver error during 4.14.98 Linux kernel bootup on imx6 SoM :

OF: /soc/aips-bus@02100000/i2c@021a0000/touch@0x10: could not get #reset-cells for /soc/aips-bus@02000000/gpio@020b0000

with the following device tree following GPIO Reset controller 

 

/
{
	fusion_reset: reset-controller {
		compatible = "gpio-reset";
		reset-gpios = <&gpio6 2 GPIO_ACTIVE_HIGH>;
		reset-delay-us = <10000>;
		#reset-cells = <0>;
	};
};

&i2c1 {		
	status = "okay";
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c1_mercury
			&pinctrl_touch_mercury>;

    fusion_touch: touch@0x10{
		compatible = "fusion-ts";
		reg = <0x10>;
		interrupts-extended = <&gpio7 12 IRQ_TYPE_EDGE_RISING>; 
		resets = <&fusion_reset>;
		//status = "okay";
	};
}; 
&fusion_touch {
	status = "okay";
};

 

 

Any pointers on what's going on here?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

1,164件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello nxpsri,

 

You must be using the I2C in another instance since there's no error in your device tree, what error do you see in your console?

Regards

 

0 件の賞賛
返信