Full UART sample cord using GPIO for i.MX6DL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Full UART sample cord using GPIO for i.MX6DL

跳至解决方案
1,256 次查看
yuuki
Senior Contributor II

Dear all,

We use i.MX6DL and Linux BSP(L4.1.15_2.0.0).
We understand that only UART1 is Full-UART.

However, we want to use UART2 as Full UART.
We want to control DCD, DSR, DTR, RI in SW by using GPIO.

Does such a sample cord exist?

Best Regards,
Yuuki

标签 (2)
标记 (6)
0 项奖励
回复
1 解答
1,157 次查看
b36401
NXP Employee
NXP Employee

Accordingly to table 64-2 of the Reference Manual only UART1 has DCD, DSR, RTS and RI signals connected to chip pads.
We have no sample cord for UART2.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,158 次查看
b36401
NXP Employee
NXP Employee

Accordingly to table 64-2 of the Reference Manual only UART1 has DCD, DSR, RTS and RI signals connected to chip pads.
We have no sample cord for UART2.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复