Full UART sample cord using GPIO for i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full UART sample cord using GPIO for i.MX6DL

ソリューションへジャンプ
1,214件の閲覧回数
yuuki
Senior Contributor II

Dear all,

We use i.MX6DL and Linux BSP(L4.1.15_2.0.0).
We understand that only UART1 is Full-UART.

However, we want to use UART2 as Full UART.
We want to control DCD, DSR, DTR, RI in SW by using GPIO.

Does such a sample cord exist?

Best Regards,
Yuuki

ラベル(2)
タグ(6)
0 件の賞賛
返信
1 解決策
1,115件の閲覧回数
b36401
NXP Employee
NXP Employee

Accordingly to table 64-2 of the Reference Manual only UART1 has DCD, DSR, RTS and RI signals connected to chip pads.
We have no sample cord for UART2.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,116件の閲覧回数
b36401
NXP Employee
NXP Employee

Accordingly to table 64-2 of the Reference Manual only UART1 has DCD, DSR, RTS and RI signals connected to chip pads.
We have no sample cord for UART2.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信