Full UART sample cord using GPIO for i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Full UART sample cord using GPIO for i.MX6DL

Jump to solution
2,075 Views
yuuki
Senior Contributor I

Dear all,

We use i.MX6DL and Linux BSP(L4.1.15_2.0.0).
We understand that only UART1 is Full-UART.

However, we want to use UART2 as Full UART.
We want to control DCD, DSR, DTR, RI in SW by using GPIO.

Does such a sample cord exist?

Best Regards,
Yuuki

Labels (2)
Tags (5)
0 Kudos
Reply
1 Solution
1,976 Views
b36401
NXP Employee
NXP Employee

Accordingly to table 64-2 of the Reference Manual only UART1 has DCD, DSR, RTS and RI signals connected to chip pads.
We have no sample cord for UART2.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,977 Views
b36401
NXP Employee
NXP Employee

Accordingly to table 64-2 of the Reference Manual only UART1 has DCD, DSR, RTS and RI signals connected to chip pads.
We have no sample cord for UART2.
Sorry for the inconvenience.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply