I'm using android 4.4.2/imx6q. I have frequent binder error with frequent random crash (null pointer crash usually) when plying with android GUI.
Here is an example of the binder error:
[ 137.361335] binder: release proc 3628, transaction 25361, not freed
[ 137.367610] binder: release proc 3628, transaction 25388, not freed
[ 162.268018] binder: 3182:3182 transaction failed 29189, size 92-0
[ 174.459282] binder: release 2297:2345 transaction 30308 in, still active
[ 174.466001] binder: send failed reply for transaction 30308 to 3057:3075
[ 174.474214] binder: release 2297:3257 transaction 30299 in, still active
[ 174.483290] binder: send failed reply for transaction 30299 to 3870:3870
[ 174.490148] binder: release proc 2297, transaction 30309, not freed
[ 174.496757] request_suspend_state: wakeup (0->0) at 174258127689 (1970-01-02 00:29:57.974331687 UTC)
[ 174.529938] init: untracked pid 3505 exited
[ 174.559633] init: untracked pid 3689 exited
[ 174.589377] init: untracked pid 3482 exited
[ 174.593865] init: untracked pid 3373 exited
[ 174.598194] init: untracked pid 3410 exited
[ 174.608484] init: untracked pid 3430 exited
[ 174.616773] init: untracked pid 3229 exited
[ 174.622210] init: untracked pid 3316 exited
[ 174.628353] init: untracked pid 3445 exited
[ 174.634000] init: untracked pid 3182 exited
[ 174.639448] init: untracked pid 3212 exited
[ 174.645194] init: untracked pid 3195 exited
[ 174.653668] init: untracked pid 3113 exited
[ 174.659857] init: untracked pid 3262 exited
[ 174.665214] init: untracked pid 3279 exited
[ 174.670170] init: untracked pid 3462 exited
[ 174.674735] init: untracked pid 3538 exited
[ 174.679930] init: untracked pid 3057 exited
[ 174.759346] init: untracked pid 3870 exited
[ 174.839368] alarm_release: clear alarm, pending 0
[ 174.844092] alarm_release: clear alarm, pending 0
[ 175.003312] binder: 3057: binder_alloc_buf, no vma
[ 175.008343] binder: 4008:4104 transaction failed 29201, size 124-4
[ 175.015018] binder: 3057: binder_alloc_buf, no vma
[ 175.019899] binder: 4008:4104 transaction failed 29201, size 124-4
The issue is solved. The errors were caused by DRAM issue.
Hi. oussama.
I had an issue similar to you.
I wonder how you solved the DRAM issue.
Hello, 
Wondering, is there an answer to the DRAM issue?  How was it solved?  Thank you
Hello Oussama.
The GUI works without problems rigth?, but you still get the error correct?
There could be a lot of reasons for this, but probably android init is trying to initialize a specific service and it is failing.
I would recommend you to check the logcat (it most probably be a huge file) and you could find the program that is constantly crashing.
Have a great day,
Sergio
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Sergio,
Each time the GUI crash and restart, there are fatal signal like signal 11, singal 7.
Example:
F/libc ( 2283): invalid address or address of corrupt block 0x2b357b54 passed to dlfree
F/libc ( 2283): Fatal signal 7 (SIGBUS) at 0x00000000 (code=128), thread 2321 (Binder_2)
I/DEBUG ( 2282): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 2282): Build fingerprint: 'Freescale/xxxx/xxxx:4.4.2/0.0.1/20150102:eng/dev-keys'
I/DEBUG ( 2282): Revision: '405525'
I/DEBUG ( 2282): pid: 2283, tid: 2321, name: Binder_2 >>> /system/bin/surfaceflinger <<<
I/DEBUG ( 2282): signal 7 (SIGBUS), code 128 (SI_KERNEL), fault addr 00000000
I/DEBUG ( 2282): Abort message: 'invalid address or address of corrupt block 0x2b357b54 passed to dlfree'
OR
F/libc ( 3781): Fatal signal 11 (SIGSEGV) at 0x00000400 (code=1), thread 4073 (android.browser)
I/DEBUG ( 3896): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 3896): Build fingerprint: 'Freescale/xxxx/xxxx:4.4.2/0.0.1/20150102:eng/dev-keys'
I/DEBUG ( 3896): Revision: '405525'
I/DEBUG ( 3896): pid: 3781, tid: 4073, name: android.browser >>> com.android.browser <<<
I/DEBUG ( 3896): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 00000400
OR
F/libc ( 2274): invalid address or address of corrupt block 0x34e95b54 passed to dlfree
F/libc ( 2274): Fatal signal 7 (SIGBUS) at 0x00000000 (code=128), thread 3231 (Binder_3)
I/DEBUG ( 2273): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 2273): Build fingerprint: 'Freescale/xxxx/xxxx:4.4.2/0.0.1/20150102:eng/dev-keys'
I/DEBUG ( 2273): Revision: '405525'
I/DEBUG ( 2273): pid: 2274, tid: 3231, name: Binder_3 >>> /system/bin/surfaceflinger <<<
I/DEBUG ( 2273): signal 7 (SIGBUS), code 128 (SI_KERNEL), fault addr 00000000
I/DEBUG ( 2273): Abort message: 'invalid address or address of corrupt block 0x34e95b54 passed to dlfree'
OR
F/libc ( 2277): Fatal signal 11 (SIGSEGV) at 0x0000041c (code=1), thread 3053 (Binder_2)
I/DEBUG ( 2273): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***
I/DEBUG ( 2273): Build fingerprint: 'Freescale/xxxx/xxxx:4.4.2/0.0.1/20150102:eng/dev-keys'
I/DEBUG ( 2273): Revision: '405525'
I/DEBUG ( 2273): pid: 2277, tid: 3053, name: Binder_2 >>> /system/bin/mediaserver <<<
I/DEBUG ( 2273): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 0000041c
Any clue who cause this bad memory access on the kernel and userspace?
Have a Great Day!
Oussama
Have you seen this behaviour with any other FSL BSP you have built?