I'm using android 4.4.2/imx6q. I have frequent binder error with frequent random crash (null pointer crash usually) when plying with android GUI.
Here is an example of the binder error:
[ 137.361335] binder: release proc 3628, transaction 25361, not freed
[ 137.367610] binder: release proc 3628, transaction 25388, not freed
[ 162.268018] binder: 3182:3182 transaction failed 29189, size 92-0
[ 174.459282] binder: release 2297:2345 transaction 30308 in, still active
[ 174.466001] binder: send failed reply for transaction 30308 to 3057:3075
[ 174.474214] binder: release 2297:3257 transaction 30299 in, still active
[ 174.483290] binder: send failed reply for transaction 30299 to 3870:3870
[ 174.490148] binder: release proc 2297, transaction 30309, not freed
[ 174.496757] request_suspend_state: wakeup (0->0) at 174258127689 (1970-01-02 00:29:57.974331687 UTC)
[ 174.529938] init: untracked pid 3505 exited
[ 174.559633] init: untracked pid 3689 exited
[ 174.589377] init: untracked pid 3482 exited
[ 174.593865] init: untracked pid 3373 exited
[ 174.598194] init: untracked pid 3410 exited
[ 174.608484] init: untracked pid 3430 exited
[ 174.616773] init: untracked pid 3229 exited
[ 174.622210] init: untracked pid 3316 exited
[ 174.628353] init: untracked pid 3445 exited
[ 174.634000] init: untracked pid 3182 exited
[ 174.639448] init: untracked pid 3212 exited
[ 174.645194] init: untracked pid 3195 exited
[ 174.653668] init: untracked pid 3113 exited
[ 174.659857] init: untracked pid 3262 exited
[ 174.665214] init: untracked pid 3279 exited
[ 174.670170] init: untracked pid 3462 exited
[ 174.674735] init: untracked pid 3538 exited
[ 174.679930] init: untracked pid 3057 exited
[ 174.759346] init: untracked pid 3870 exited
[ 174.839368] alarm_release: clear alarm, pending 0
[ 174.844092] alarm_release: clear alarm, pending 0
[ 175.003312] binder: 3057: binder_alloc_buf, no vma
[ 175.008343] binder: 4008:4104 transaction failed 29201, size 124-4
[ 175.015018] binder: 3057: binder_alloc_buf, no vma
[ 175.019899] binder: 4008:4104 transaction failed 29201, size 124-4