Freescale Linux 2.6-imx.git Fatal Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale Linux 2.6-imx.git Fatal Error

1,692件の閲覧回数
ThanarajS
Contributor III

Hi All,

We are trying to git freescale linux-imx.git code but we were not able to download the kernel code for Android 7.

Is there any server issue in Freescale linux-imx?

Last Two days we are getting below error,

root@cpu-493-PC:/work/myandroid# git clone git://git.freescale.com/imx/linux-imx.git kernel_imx
Cloning into 'kernel_imx'...
fatal: repository 'https://git.freescale.com/imx/linux-imx.git/' not found


root@cpu-493-PC:/work/myandroid# git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx
Cloning into 'kernel_imx'...
fatal: repository 'https://git.freescale.com/imx/linux-2.6-imx.git/' not found
root@cpu-493-PC:/work/myandroid#

Thanks

Regards,

Raj.

Regards,
Thanaraj Subramani
ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,396件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi, we are working internally to get this resolved.   The GIT managers are aware of the issue and we are working to find the root cause and solution.  In the meantime, you can navigate to the GIT website in web browser and download packages from there.   We hope to have it resolved soon.


Best regards,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,396件の閲覧回数
ko-hey
Senior Contributor II

Hi @Carlos_Musich

I had a same problem now.

Have it already resolved ?

Ko-hey

0 件の賞賛
返信