Hi all,
I am trying a decoding of H.264 video on i.MX6Q Sabre board using Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga).
But, some of the frames are dropped when I try decoding and scaling.
[Command]
> gst-launch-1.0 filesrc location=test_640x480.avi typefind=true ! video/x-msvideo ! aiurdemux ! vpudec ! videoscale method=1 ! video/x-raw,width=800,height=480 ! overlaysink
[Error Message]
> WARNING: from element /GstPipeline:pipeline0/GstOverlaySink:overlaysink0: A lot of buffers are being dropped.
> Additional debug info:
build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/gstreamer1.0/1.4.5-r0/gstreamer-1.4.5/libs/gst/base/gstbasesink.c(2794): gst_base_sink_is_too_late (): /GstPipeline:pipeline0/GstOverlaySink:overlaysink0:
> There may be a timestamping problem, or this computer is too slow.
When I try only the decoding and only the scaling, there are not dropped frame.
I think that "vpudec" is hardware-based process and "videoscale" is software-based process.
Therefore, I think that the decoding and the scaling can be parallel processing.
Why some of the frame is dropped?
As additional information, I measure the processing time.
With decoding : Scaling time is 61ms / frame
Only Scaling (*) : Scaling time is 8ms / frame
(*) YUV showing (No decoding)
Command : gst-launch-1.0 filesrc location=test_640x480.yuv ! videoparse format=2 width=640 height=480 framerate=15 ! videoscale method=1 ! video/x-raw,width=800,height=480 ! overlaysink
Why the scaling time is long when decoding and scaling has been processed at the same time?
Best Regards,
Kenji
Hello,
  Looks like the issue is just a performance issue, mainly because of software “videoscale”. 
Please try using one of video conversion plugins (imxvideoconvert_ipu, imxvideoconvert_g2d, 
imxvideoconvert_pxp) to resize image. 
  Also You may try to insert queue element in Gstreamer pipeline for buffering in order to 
improve situation.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Yuri,
Thank you so much for your comment.
I am using the i.MX6Q Sabre board. Therefore, in this case, the software "videoscale" is runing on 1GHz ARM Cortex-A9 processor.
I checked "videoscale" source code, and I think that this processing throughput is not large.
So, I think the performance is enough for "videoscale".
What do you think about this?
BTW, about imxvideoconvert_ipu or imxvideoconvert_g2d, does these plugins have the resize function?
Please tell me a command to resize about these plugin.
I appreciate your cooperation.
Best Regards,
Kenji
   Please try  imxvideoconvert_ipu or imxvideoconvert_g2d, using section 
 7.3.15 (Video conversion) of "i.MX_Linux_User's_Guide.pdf".
Also, perhaps it is possible to use more speedy file storage device.
Regards,
Yuri.
Dear Yuri,
Thank you so much for your replay.
I was successful according to the manual. Thank you!
About this, do you know the scaling method about imxvideoconvert_ipu or imxvideoconvert_g2d? bicubic or bilinear? The specified is possible?
BTW,
> I am using the i.MX6Q Sabre board. Therefore, in this case, the software "videoscale" is runing on 1GHz ARM Cortex-A9 processor.
> So, I think the performance is enough for "videoscale".
What do you think about this?
Best Regards,
Kenji
Hello,
You may look at sources ; please refer to "i.MX_Linux_Release_Notes.pdf" to define
what package contains GStreamer plugins.
As for performance it depends on application.
Regards,
Yuri.
Hello Yuri,
Thank you for your comments.
I can not find the source code of imxvideoconvert_ipu and imxvideoconvert_g2d plugins.
I think that this code is private firmware and binary code.
> As for performance it depends on application.
I am using the original i.MX6Q Sabre board and original Freescale Yocto Project BSP code (imx-3.14.52-1.1.0_ga).
And, I am using "fsl-image-qt5" image.
I do not know why the performance is bad.
Best Regards,
Kenji