Frambuffer rotation i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frambuffer rotation i.MX6

989 Views
wesleyrevens
Contributor I

I have a TN LCD screen where the viewing angles are much improved if I turn the screen upside down.

Unfortunately, that means I also need to be able to rotate the graphics output by 180 degrees.

If I run "echo  3 > /sys/devices/soc0/fb.23/graphics/fb0/rotate" which should be an IPU_ROTATE_180

The image is not rotated.

The only time I get a change in the image on the screen is if I echo 1 > /sys/devices/soc0/fb.23/graphics/fb0/rotate

but that maps to IPU_VERT_FLIP so the image still looks incorrect on my screen.

Can anyone tell me how to get the IPU rotations >= 2 To work? I'm using kernel 3.14.38

Labels (1)
0 Kudos
Reply
1 Reply

714 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wesley

please look at link below where is is discussed in details

https://community.freescale.com/message/567360#567360

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply