For i.MX7 processor, how to interface rotational speed sensors with isolation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For i.MX7 processor, how to interface rotational speed sensors with isolation?

842件の閲覧回数
sourabhzunke090
Contributor I

Which port should be used for interfacing speed sensors with frequency range output of 1Hz- 20KHZ?

ラベル(3)
0 件の賞賛
返信
1 返信

792件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi sourabh

one can consider timers, gpt or flextimer described in

Chapter 12 Timers i.MX7 Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信