For i.MX7 processor, how to interface rotational speed sensors with isolation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For i.MX7 processor, how to interface rotational speed sensors with isolation?

917 Views
sourabhzunke090
Contributor I

Which port should be used for interfacing speed sensors with frequency range output of 1Hz- 20KHZ?

Labels (3)
0 Kudos
Reply
1 Reply

867 Views
igorpadykov
NXP Employee
NXP Employee

Hi sourabh

one can consider timers, gpt or flextimer described in

Chapter 12 Timers i.MX7 Reference Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply