Hi NXP,
 
(1)I'm trying to building yocto i.MX8 32-bit applications on 64-bit OS. 
 
 
(2)Reference L5.4.70_2.3.0 i.MX Yocto Project User's Guide
 
 
(3)I'm trying bitbake imx-image-full.
 
The error message is almost like this:
 
| ninja: build stopped: subcommand failed.
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (virtual:native:/home/adv/adv-release-bsp-new/sources/meta-clang/recipes-devtools/clang/clang_git.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 6324 tasks of which 6203 didn't need to be rerun and 2 failed.
 
Summary: 2 tasks failed:
  /home/adv/adv-release-bsp-new/sources/poky/meta/recipes-devtools/python/python3-nose_1.3.7.bb:do_patch
  virtual:native:/home/adv/adv-release-bsp-new/sources/meta-clang/recipes-devtools/clang/clang_git.bb:do_compile
Summary: There were 2 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
 
Can you please help?
 
Thank you,