For Upgrade Android jb4.3 ga with the latest GPU driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For Upgrade Android jb4.3 ga with the latest GPU driver

ソリューションへジャンプ
2,294件の閲覧回数
yuuki
Senior Contributor II

Our customer referred to the following information and tried it.

https://community.freescale.com/docs/DOC-100351#comment-10841

However, the "Android.mk.def" is not found, which is described in drivers/mxc/gpu-viv/hal/kernel/Android.mk file.
They cannot build.

May I have advice?

Best Regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,935件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Hi,

From the document owner:

"It is galcore build-out makefile, not used in built-in kernel, I removed it in the updated package,

you can ask customer to sync the latest package, or remove drivers/mxc/gpu-viv/hal/Android.mk file directly."

Michel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,936件の閲覧回数
ChucoChe
NXP Employee
NXP Employee

Hi,

From the document owner:

"It is galcore build-out makefile, not used in built-in kernel, I removed it in the updated package,

you can ask customer to sync the latest package, or remove drivers/mxc/gpu-viv/hal/Android.mk file directly."

Michel

0 件の賞賛
返信
1,935件の閲覧回数
yuuki
Senior Contributor II

Dear Michel,

Thank you for your help.

Our customer succeeded in building.

Beset Regards,

0 件の賞賛
返信