DDR3 clock domain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR3 clock domain

2,104件の閲覧回数
pscz
Contributor II

Hello,

I've been working on the hardware of a board with a 4core i.MX6.

I have 4 memory chip, all DDR3.

From the reference design (MCIMX6Q-SMART DEVICE BOARD, pag. 4), I see that:

- two DDR3 modules are connected to DRAM_SDCLK0

- two DDR3 modules are connected to DRAM_SDCLK1

The clock enable used is DRAM_SDCKE0 while DRAM_SDCKE1 is unconnected.

Also DRAM_SDODT0 controls the on-die termination of all the four modules while DRAM_SDODT1 is unconnected.

Can anyone explain why?

Thank you in advance,

Alessandro

ラベル(2)
0 件の賞賛
返信
1 返信

1,824件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi alesandro,

on MCIMX6Q-SMART DEVICE BOARD, pag. 4

all 4 memory chip, all DDR3 are connected to DRAM_CS0,

so DRAM_SDCKE1,DRAM_SDODT1 are not used (they are used

with  DRAM_CS0). However DRAM_SDCLK0,DRAM_SDCLK1 is the

same signal (duplicates each other).

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信