For Status Code of i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For Status Code of i.MX53

Jump to solution
1,416 Views
yuuki
Senior Contributor II


Dear, all

I refer to 7.8.3 Serial Download Protocol in Reference Manual.
  iMX53RM.pdf(Rev2.1) P.529-

There is Description about Status Code in Section 7.8.3.1 Get Status.
However, the detail description about the contents of Status Code does not occur.

May I have a Status Code detail description?

For example,
- What does "F0" mean?
- What does "33" mean?

Best Regards,

Labels (1)
0 Kudos
Reply
1 Solution
1,286 Views
Yuri
NXP Employee
NXP Employee

Please use Table 7-21 (HAB Status Codes) of i.MX25 Reference Manual.

http://cache.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,287 Views
Yuri
NXP Employee
NXP Employee

Please use Table 7-21 (HAB Status Codes) of i.MX25 Reference Manual.

http://cache.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply