For Status Code of i.MX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For Status Code of i.MX53

ソリューションへジャンプ
1,950件の閲覧回数
yuuki
Senior Contributor II


Dear, all

I refer to 7.8.3 Serial Download Protocol in Reference Manual.
  iMX53RM.pdf(Rev2.1) P.529-

There is Description about Status Code in Section 7.8.3.1 Get Status.
However, the detail description about the contents of Status Code does not occur.

May I have a Status Code detail description?

For example,
- What does "F0" mean?
- What does "33" mean?

Best Regards,

ラベル(1)
0 件の賞賛
返信
1 解決策
1,820件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use Table 7-21 (HAB Status Codes) of i.MX25 Reference Manual.

http://cache.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,821件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please use Table 7-21 (HAB Status Codes) of i.MX25 Reference Manual.

http://cache.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信