FlexSPI supported serial clock frequencies in i.MX 8X processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexSPI supported serial clock frequencies in i.MX 8X processor

1,336 次查看
syuriks
Contributor I

Hello,

I need clarification regarding FlexSPI supported serial clock frequencies in i.MX 8X processor. As far as I could understand FlexSPI clock serialClkFreq is configured by ROM and its frequencies vary from 20 to 200 MHz.

The question is whether serialClkFreq and flexspi0_ipg_clk_sfck/flexspi1_ipg_clk_sfck is the same clock? Based on MCR0 register serial root clock can be divided maximum by 8. Does it mean that the minimum supported frequency is 2.5MHz?

Thanks,

Yuri

0 项奖励
回复
1 回复

1,211 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yuri

supported frequencies are described in i.MX8QXP Datasheet

sect.4.10.12 FlexSPI timing parameters:
The FlexSPI interface can work in SDR or DDR modes. It can operate

up to 60 MHz at 3.3 V, 166 MHz at 1.8 V SDR mode

https://www.nxp.com/docs/en/data-sheet/IMX8QXPAEC.pdf

There is no min.frequency limit, as for "2.5MHz" - one can consider

various parents clocks with dividers in Chapter 8 Clocking i.MX8DQXP Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX8DQXPRM.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复