Build IMAX8M Yocto environment task error problem!!!!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Build IMAX8M Yocto environment task error problem!!!!

1,576 Views
egbert8165
Contributor I

Hi NXP Team,

I executed the bitbake fsl-image-qt5-validation-imx command following instructions but found a problem (reger below Figure).

3.jpg

After executing the bitbake-c fetchall fsl-image-qt5-validation-imx command and executed the bitbake fsl-image-qt5-validation-imx  to rebuilding it, the following error message still appears. How can I solve this problem? (refer below Figure )

4.jpg

5.jpg

BR

Egbert Liu

Tags (1)
0 Kudos
Reply
1 Reply

1,496 Views
igorpadykov
NXP Employee
NXP Employee

Hi Egbert 

for building image with QT5 one can look on

wayland image with QT5 fails to build on Yocto Rocko for i.mx8m 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply