Flashing issues with wic image using UUU tool on windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing issues with wic image using UUU tool on windows

1,224 Views
mallikarjuna
Contributor II

Hi,

I am flashing .wic image of 3GB or more(Tried upto 20GB) on IMX8M plus processor based custom board using UUU tool on windows and facing below error "Bulk(W): LIBUSB_ERROR_PIPE (-9)" . Please find attached image for error 

mallikarjuna_0-1729242425160.png

 

UUU tool version that we are using :

UUU tool version :-  libuuu_1.5.182-0-gda3cd53 

 

Can you please help us on these issue ? 

0 Kudos
Reply
3 Replies

1,177 Views
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @mallikarjuna 

You can try to flashing also your sd.flash file.

Command:

uuu -c emmc_all <bootloader_sd.flash> <image.wic>

 

Please let me know if this worked for you.

 

Best regards,

Salas.

0 Kudos
Reply

579 Views
Ludek_Zaloudek
NXP Employee
NXP Employee

Hello @Manuel_Salas , did you manage to find out what was the cause of the -9 error? I have just encountered the same issue with an i.MX9XX board. To me, this appears as a HW issue, as I was able to use the UUU SD-card upload on one board but not on the other (same type, just different DDR).

With regards

Ludek

0 Kudos
Reply

1,145 Views
mallikarjuna
Contributor II

Hi @Manuel_Salas ,

 

We are flashing compressed .wic.zst file which contains u-boot binaries, kernel image and root filesystem I think, so no need to flash bootloader_sd.flash file seperately, Right ?.

 

Our wic.zst file size is 293MB only, if we extract that file .wic size is 3GB. 


If .wic size is more that 2.5gb and  we are trying to flash i n our IMX8m plus based custom board, it's giving bulk error like these "Bulk(W): LIBUSB_ERROR_PIPE (-9)".  

 

Can I know exact reason for Bulk error ? Is there is any max limit for .wic size to flash without Bulk(W) error ? 

This error is because of uuu tool that we are using (or) any limitation from driver/hardware side  ?

 

Thanks, 

Mallikarjuna Reddy Ambati

0 Kudos
Reply