Flashing NAND using i.mx6ull over Serial UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing NAND using i.mx6ull over Serial UART

1,920件の閲覧回数
srishan
Contributor III

Dear I.MX Community,

In my custom design we dont have USB or SD card,  but I need to flash the images using UART to NAND flash, Atleast I want to falsh the U-boot to NAND flash and then later over the network and NFS and flash the other images like dtb, zimage and rootfs

Could you please share the NXP procedure over for flashing the U-boot to NAND flash using UART

Kindly do the needful as early as possible, as I am stuck with this from past many days

Many Thanks in advance

Eagerly awaiting for your replies

ラベル(2)
0 件の賞賛
返信
1 返信

1,627件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could take a look at the links below regarding complementary information about implementation of UART serial downloader for i.MX processors:

https://www.nxp.com/docs/en/application-note/AN3996.pdf

https://community.nxp.com/docs/DOC-1639

https://github.com/boundarydevices/imx_usb_loader


Hope this will be useful for you.
Best regards!
/Carlos

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信