downloading the images to NAND over UART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

downloading the images to NAND over UART

952 次查看
srishan
Contributor III

Dear I.mX Community,

i.MX 6ULL Applications Processor Reference Manual, Rev. 1, 11/2017 says that images can be downloaded using UART as  mentioned in section 8.2.4 Serial Downloader using UART


Could you please let me know, whether UART is enabled in ROM in serial downloader mode for loading images to NAND flash instead of USB??

Could you please share the procedure for downloading the images over UART to NAND flash

Kindly do the needful as early as possible as am stuck with this frm past many days, No clues till as of now

Thanks in advance,

标签 (2)
0 项奖励
回复
1 回复

769 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could take a look at the links below regarding complementary information about implementation of UART serial downloader for i.MX processors:

https://www.nxp.com/docs/en/application-note/AN3996.pdf

https://community.nxp.com/docs/DOC-1639

https://github.com/boundarydevices/imx_usb_loader


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复