Flashing Android 9 build images to imx8 mini using uuu tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flashing Android 9 build images to imx8 mini using uuu tool

1,754件の閲覧回数
nxf40102
NXP Employee
NXP Employee

Hi,

I have setup an AOSP build environment of Android 9 for imx8 Mini. I followed the instruction given in User guide. 

I am able to build complete AOSP successfully. but while flashing freshly build images to imx 8Mini i am facing below issue.

I have used uuu_imx_android_flash.bat file to flash, below is the message 

>uuu_imx_android_flash.bat -f imx8mm -a -e
This script is validated with uuu 1.2.135 version, please align with this version.
dtbo is supported
dual slot is supported
You do not have sufficient privilege to perform this operation.

I am not able to understand what i am doing wrong. Instead of freshly build images if I use prebuild images its flashing properly.

ラベル(3)
0 件の賞賛
返信
1 返信

1,487件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

it seems that this needs administrative privilege to operate, if you don't have this right, maybe you can run under ubuntu

0 件の賞賛
返信