Flash with imx8mp EVK board with uuu

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flash with imx8mp EVK board with uuu

ソリューションへジャンプ
5,503件の閲覧回数
arno_0
Contributor III

Try to download full image to internal emmc by uuu.

It looks like as uuu -v -V uuu.auto-imx8mpevk would do the job.

It starts and I get some info in windows console and in device console, but than it stucks at fastboot. Something I do wrong?

Attached the logs.

The expected result would be to boot in internal emmc same as it would from sdcard.

0 件の賞賛
返信
1 解決策
5,480件の閲覧回数
arno_0
Contributor III

Knowing it should work I checked that all again. Your log doesn't provide much information. But looking to mines - I miss the imx8mp there.

So the reason simply was an old outdated "uuu". With a new one it runs without a problem.

元の投稿で解決策を見る

8 返答(返信)
5,496件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Arno Steffens,

Could you please share me the link where you downloaded the image?

Best regards.

0 件の賞賛
返信
5,493件の閲覧回数
arno_0
Contributor III

From here:
https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

 

The image of the rootfs is rather huge, 5...9GB. Does I just need to wait a long time? But I can't see any progress even with -v parameter.

What does this fastboot mean? I see the board booting into uboot at least. But how to go on from there?

0 件の賞賛
返信
5,486件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Arno Steffens,

Yes. it is necessary to wait that time.

The recommended parameter is -b, please try with the parameter -b

uuu -b uuu.auto-imx8mpevk

Jorge7u7_0-1671473286696.png

It should work fine; it takes around 2 minutes to flash the board.

Best regards.

5,481件の閲覧回数
arno_0
Contributor III

Knowing it should work I checked that all again. Your log doesn't provide much information. But looking to mines - I miss the imx8mp there.

So the reason simply was an old outdated "uuu". With a new one it runs without a problem.

5,470件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Dear Arno Steffens,

Thank you for the feedback.

Best regards.

0 件の賞賛
返信
3,108件の閲覧回数
KLuis
Contributor I

I tried the solution, but flashing with UUU was still unsuccessful. I used VirtualBox to run my terminal and setup NXP OTG USB with USB2.0 controller in VirtualBox. I suspect the problem in my case was caused by losing the connection with NXP OTG after "Run Fast Boot" started. Can you help me to resolve the issue? Thanks.

KLuis_0-1734388827117.png

$ lsusb
Bus 002 Device 009: ID 1fc9:0146 NXP Semiconductors SE Blank 865
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 80ee:0021 VirtualBox USB Tablet
Bus 001 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub

$ lsusb
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 80ee:0021 VirtualBox USB Tablet
Bus 001 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub

---------------------------

sudo uuu -b uuu.auto-imx8mp-lpddr4-evk

uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193

Success 0 Failure 0


2:1 1/ 1 [=================100%=================] SDPS: boot -f imx-boot-im

---------------------------

$ sudo uuu -v -V uuu.auto-imx8mp-lpddr4-evk

uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193

 

Build in config:

                Pctl       Chip                    Vid        Pid        BcdVersion

                ==================================================

                SDPS:  MX8QXP                           0x1fc9               0x012f               [0x0002..0xffff]

                SDPS:  MX8QM                            0x1fc9               0x0129              [0x0002..0xffff]

                SDPS:  MX8DXL                           0x1fc9               0x0147

                SDPS:  MX28                  0x15a2              0x004f

                SDPS:  MX815                               0x1fc9               0x013e

                SDPS:  MX865                               0x1fc9               0x0146

                SDPS:  MX8ULP                           0x1fc9               0x014a

                SDPS:  MX8ULP                           0x1fc9               0x014b

                SDP:     MX7D                 0x15a2              0x0076

                SDP:     MX6Q                 0x15a2              0x0054

                SDP:     MX6D                 0x15a2              0x0061

                SDP:     MX6SL                               0x15a2              0x0063

                SDP:     MX6SX                               0x15a2              0x0071

                SDP:     MX6UL                              0x15a2              0x007d

                SDP:     MX6ULL                            0x15a2              0x0080

                SDP:     MX6SLL                            0x1fc9               0x0128

                SDP:     MX7ULP                           0x1fc9               0x0126

                SDP:     MXRT106X      0x1fc9               0x0135

                SDP:     MX8MM                            0x1fc9               0x0134

                SDP:     MX8MQ                            0x1fc9               0x012b

                SDPU: SPL                      0x0525              0xb4a4              [0x0000..0x04ff]

                SDPV:  SPL1                   0x0525              0xb4a4              [0x0500..0x9998]

                SDPV:  SPL1                   0x1fc9               0x0151              [0x0500..0x9998]

                SDPU: SPL                      0x0525              0xb4a4              [0x9999..0x9999]

                SDPU: SPL                      0x3016              0x1001              [0x0000..0x04ff]

                SDPV:  SPL1                   0x3016              0x1001              [0x0500..0x9998]

                FBK:                                     0x066f               0x9afe

                FBK:                                     0x066f               0x9bff

                FBK:                                     0x1fc9               0x0153

                FB:                                        0x0525              0xa4a5

                FB:                                        0x18d1              0x0d02

                FB:                                        0x3016              0x0001

                FB:                                        0x1fc9               0x0152

Wait for Known USB Device Appear...

New USB Device Attached at 2:1

2:1>Start Cmd:SDPS: boot -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk

100%2:1>Okay (6.09s)

---------------------------

U-Boot SPL 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)

DDRINFO: start DRAM init

DDRINFO: DRAM rate 4000MTS

DDRINFO:ddrphy calibration done

DDRINFO: ddrmix config done

SEC0:  RNG instantiated

Normal Boot

Trying to boot from BOOTROM

Boot Stage: USB boot

Find img info 0x48022fa0, size 1064

Need continue download 1024

NOTICE:  Do not release JR0 to NS as it can be used by HAB

NOTICE:  BL31: v2.10.0  (release):android-14.0.0_2.0.0-rc1-1-g49143a170

NOTICE:  BL31: Built : 10:04:22, May 29 2024

 

 

U-Boot 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)

 

CPU:   i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)

CPU:   Commercial temperature grade (0C to 95C) at 40C

Reset cause: POR

Model: NXP i.MX8MPlus LPDDR4 EVK board

DRAM:  6 GiB

TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]

Power supply on USB2

TCPC:  Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]

Core:  287 devices, 37 uclasses, devicetree: separate

MMC:   FSL_SDHC: 1, FSL_SDHC: 2

Loading Environment from nowhere... OK

[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c

fail to probe panel device adv7535@3d

fail to get display timings

probe video device failed, ret -19

 

        [0] lcd-controller@32e80000, video

        [1] mipi_dsi@32e60000, video_bridge

        [2] adv7535@3d, panel

adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c

fail to probe panel device adv7535@3d

fail to get display timings

probe video device failed, ret -19

In:    serial

Out:   serial

Err:   serial

SEC0:  RNG instantiated

switch to partitions #0, OK

mmc1 is current device

Detect USB boot. Will enter fastboot mode!

Net:   eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]

Fastboot: Normal

Boot from USB for mfgtools

*** Warning - Use default environment for                                mfgtools

, using default environment

 

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;

Hit any key to stop autoboot:  0

 

## Checking Image at 43800000 ...

Unknown image format!

Run fastboot ...

タグ(1)
0 件の賞賛
返信
2,624件の閲覧回数
ash_
Contributor I

Hi, Could you already resolve it?

タグ(1)
0 件の賞賛
返信
2,618件の閲覧回数
ash_
Contributor I
Hi @KLuis ,

I had the same problem with my locally built image for the nxp evk. After I reconnected the serial usb connection to my VM again while keeping the uuu console uninterrupted , the flashing of the image restarted automatically. And l could boot into the image. I was wondering if you figured out the problem.
0 件の賞賛
返信