Assistance Required: Movenet Pose estimation Code for NPU in imx8mp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assistance Required: Movenet Pose estimation Code for NPU in imx8mp

228 Views
adarshkv
Contributor I

Dear NXP support,

I’m trying to run movenet model (https://github.com/NXP/eiq-model-zoo/tree/main/tasks/vision/pose-estimation/movenet) on the i.MX 8M Plus NPU using libvx_delegate.so, but I’m hitting unsupported ops and a segmentation fault. Here’s the output:


Loading NPU delegate from /usr/lib/libvx_delegate.so
Vx delegate: allowed_builtin_code set to 0.
Vx delegate: error_during_init set to 0.
Vx delegate: error_during_prepare set to 0.
Vx delegate: error_during_invoke set to 0.
ERROR: Fallback unsupported op 53 to TfLite
ERROR: Fallback unsupported op 90 to TfLite
ERROR: Fallback unsupported op 53 to TfLite
ERROR: Fallback unsupported op 53 to TfLite
ERROR: Fallback unsupported op 88 to TfLite
ERROR: Fallback unsupported op 90 to TfLite
ERROR: Fallback unsupported op 53 to TfLite
ERROR: Fallback unsupported op 53 to TfLite
ERROR: Fallback unsupported op 88 to TfLite
Segmentation fault

 

I’ve attached my Python script (example_npu.py) and movenet model. It works on CPU but crashes with the NPU. 

Could you provide an updated code example for running movenet.tflite (or a similar model) on the NPU , addressing these errors? Assistance with model optimization would also help.
 
import cv2
import tensorflow as tf
import numpy as np
import time

MODEL_FILENAME = "movenet_opt.tflite"  # Use optimized model
IMAGE_FILENAME = "example_input.jpg"
LINE_COLOR = (255, 128, 0)
POINT_COLOR = (0, 0, 255)
DELEGATE_PATH = "/usr/lib/libvx_delegate.so"

keypoints_def = [...]  # Your keypoints_def and connections unchanged

# Load delegate with debugging
delegate_options = {"logging_level": "DEBUG"}  # Adjust based on NXP docs
print(f"Loading NPU delegate from {DELEGATE_PATH}")
try:
    npu_delegate = tf.lite.experimental.load_delegate(DELEGATE_PATH, delegate_options)
except ValueError as e:
    print(f"Failed to load delegate: {e}")
    exit(1)

# Initialize interpreter
interpreter = tf.lite.Interpreter(model_path=MODEL_FILENAME, experimental_delegates=[npu_delegate])
try:
    interpreter.allocate_tensors()
except RuntimeError as e:
    print(f"Failed to allocate tensors: {e}")
    exit(1)

def load_image(filename
    orig_image = cv2.imread(filename, 1)
    if orig_image is None:
        raise ValueError(f"Failed to load image: {filename}")
    image = cv2.cvtColor(orig_image, cv2.COLOR_BGR2RGB)
    image = cv2.resize(image, (192, 192))
    image = image[..., ::-1]
    image = np.expand_dims(image, axis=0)
    return orig_image, image

def run_inference(interpreter, image
    input_details = interpreter.get_input_details()
    output_details = interpreter.get_output_details()
    interpreter.set_tensor(input_details[0]['index'], image.astype(np.uint8))
    interpreter.invoke()
    return interpreter.get_tensor(output_details[0]['index']).astype(np.float32)

# Load image
try:
    orig_image, processed_image = load_image(IMAGE_FILENAME)
except ValueError as e:
    print(e)
    exit(1)

# Run inference
start = time.time()
out = run_inference(interpreter, processed_image)[0, 0, ...]
end = time.time()
print("Inference time:", (end - start) * 1000, "ms")

# Draw results
w, h = orig_image.shape[0:2]
out[:, 0] *= w
out[:, 1] *= h
for c in connections:
    i, j = c
    cv2.line(orig_image, (int(out[i, 1]), int(out[i, 0])), (int(out[j, 1]), int(out[j, 0])), LINE_COLOR, 5)
for i in range(out.shape[0]):
    cv2.circle(orig_image, (int(out[i, 1]), int(out[i, 0])), 5, POINT_COLOR, 10)

cv2.imwrite("example_output.jpg", orig_image)
cv2.imshow('Pose Estimation', orig_image)
cv2.waitKey(0)
cv2.destroyAllWindows()
0 Kudos
Reply
0 Replies