Try to download full image to internal emmc by uuu.
It looks like as uuu -v -V uuu.auto-imx8mpevk would do the job.
It starts and I get some info in windows console and in device console, but than it stucks at fastboot. Something I do wrong?
Attached the logs.
The expected result would be to boot in internal emmc same as it would from sdcard.
已解决! 转到解答。
Knowing it should work I checked that all again. Your log doesn't provide much information. But looking to mines - I miss the imx8mp there.
So the reason simply was an old outdated "uuu". With a new one it runs without a problem.
The image of the rootfs is rather huge, 5...9GB. Does I just need to wait a long time? But I can't see any progress even with -v parameter.
What does this fastboot mean? I see the board booting into uboot at least. But how to go on from there?
Dear Arno Steffens,
Yes. it is necessary to wait that time.
The recommended parameter is -b, please try with the parameter -b
uuu -b uuu.auto-imx8mpevk
It should work fine; it takes around 2 minutes to flash the board.
Best regards.
Knowing it should work I checked that all again. Your log doesn't provide much information. But looking to mines - I miss the imx8mp there.
So the reason simply was an old outdated "uuu". With a new one it runs without a problem.
I tried the solution, but flashing with UUU was still unsuccessful. I used VirtualBox to run my terminal and setup NXP OTG USB with USB2.0 controller in VirtualBox. I suspect the problem in my case was caused by losing the connection with NXP OTG after "Run Fast Boot" started. Can you help me to resolve the issue? Thanks.
$ lsusb
Bus 002 Device 009: ID 1fc9:0146 NXP Semiconductors SE Blank 865
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 80ee:0021 VirtualBox USB Tablet
Bus 001 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
$ lsusb
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 002: ID 80ee:0021 VirtualBox USB Tablet
Bus 001 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub
---------------------------
sudo uuu -b uuu.auto-imx8mp-lpddr4-evk
uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193
Success 0 Failure 0
2:1 1/ 1 [=================100%=================] SDPS: boot -f imx-boot-im
---------------------------
$ sudo uuu -v -V uuu.auto-imx8mp-lpddr4-evk
uuu (Universal Update Utility) for nxp imx chips -- lib1.4.193
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152
Wait for Known USB Device Appear...
New USB Device Attached at 2:1
2:1>Start Cmd:SDPS: boot -f imx-boot-imx8mp-lpddr4-evk-sd.bin-flash_evk
100%2:1>Okay (6.09s)
---------------------------
U-Boot SPL 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)
DDRINFO: start DRAM init
DDRINFO: DRAM rate 4000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from BOOTROM
Boot Stage: USB boot
Find img info 0x48022fa0, size 1064
Need continue download 1024
NOTICE: Do not release JR0 to NS as it can be used by HAB
NOTICE: BL31: v2.10.0 (release):android-14.0.0_2.0.0-rc1-1-g49143a170
NOTICE: BL31: Built : 10:04:22, May 29 2024
U-Boot 2024.04+g674440bc73e+p0 (Jun 06 2024 - 10:05:34 +0000)
CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 40C
Reset cause: POR
Model: NXP i.MX8MPlus LPDDR4 EVK board
DRAM: 6 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
Core: 287 devices, 37 uclasses, devicetree: separate
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from nowhere... OK
[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
fail to get display timings
probe video device failed, ret -19
[0] lcd-controller@32e80000, video
[1] mipi_dsi@32e60000, video_bridge
[2] adv7535@3d, panel
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
fail to get display timings
probe video device failed, ret -19
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
switch to partitions #0, OK
mmc1 is current device
Detect USB boot. Will enter fastboot mode!
Net: eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]
Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for mfgtools
, using default environment
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0
## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...