Flash u-boot-nand.imx to NAND

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash u-boot-nand.imx to NAND

1,737 次查看
jupiter_hce
Contributor III

Hi,

I am running a customized iMX6ULZ EVK, I am able to use kobs-ng to flash u-boot-nand.imx to NAND in Linux, has anyone used u-boot command to flash u-boot-nand.imx to NAND in u-boot instead? Or is it possible to flash u-boot-nand.imx to NAND in u-boot? Is any iMX6 document to flash u-boot-nand.imx to NAND in u-boot?

Thank you.

- jupiter

标签 (4)
标记 (1)
0 项奖励
回复
1 回复

1,544 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jupiter

nxp does not support such operations in uboot, in general one can look

at mainline uboot resources (sect.7.6. Boot from NAND Flash Memory):

Manual < DULG < DENX 

[U-Boot] [PATCH 3/3] i.MX: nand: add nandbcb update command 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复