Flash to SD2 on board Error.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash to SD2 on board Error.

跳至解决方案
1,406 次查看
cilymo
Contributor I

Hi, 

   I want to Flash the image into SD2(use OTG burn), how to do ? In imx6qsabresd borad, it can't detect the SD2 card.

error log: 

     Board: MX6-SabreSD
     I2C:   ready
     DRAM:  1 GiB
     PMIC:  PFUZE100 ID=0x10
     MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
     MMC: no card present

Thanks,

Cily

标签 (1)
0 项奖励
回复
1 解答
1,350 次查看
igorpadykov
NXP Employee
NXP Employee

Hi cily

please try with mfg tools (use mfgtool2-yocto-mx-sabresd-sdcard-sd2.vbs script)

http://www.nxp.com/webapp/Download?colCode=IMX_L4.1.15_2.1.0_MFG_TOOL&appType=license&location=null&... 

and follow atatched Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,351 次查看
igorpadykov
NXP Employee
NXP Employee

Hi cily

please try with mfg tools (use mfgtool2-yocto-mx-sabresd-sdcard-sd2.vbs script)

http://www.nxp.com/webapp/Download?colCode=IMX_L4.1.15_2.1.0_MFG_TOOL&appType=license&location=null&... 

and follow atatched Linux Guide.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复