Flash emmc on imx8mn with lpddr4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash emmc on imx8mn with lpddr4

Jump to solution
3,507 Views
bryan_hong
Senior Contributor I

hi

First, I have set SW1101 to `1000`

then, I execute below.

uuu -b emmc_all imx-boot-imx8mnevk-sd.bin-flash_evk imx-image-multimedia-imx8mnevk.tar.zst
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172

Success 0 Failure 1


5:12 1/ 1 [
HID(W):LIBUSB_ERROR_TIMEOUT ] SDPS: boot -scanterm -f imx-boot-imx8mnevk-sd.bin-flash_evk -scanlimited 0x800000

and serial port show below

U-Boot SPL 2023.04-lf_v2023.04+gaf7d004eaf (Jun 06 2023 - 14:59:40 +0000)
read error from device: 94f630 register: x!DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
Training FAILED

 

plz comment for this.

thanks

Bryan

 

 

 

0 Kudos
Reply
1 Solution
3,315 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can try other board, like 8mp, 8mm.

View solution in original post

0 Kudos
Reply
12 Replies
1,046 Views
chillinwithscb
Contributor III
There's a marking that this ticket is solved, but using a different board ("You can try other board") is not generally a workable solution.

Might be using the wrong input install file. When I build, I get both .tar.zst and .wic.zst files. I use the .wic.zst files with UUU (-b emmc_all). I don't think the .tar.zst files are directly usable via UUU.
0 Kudos
Reply
1,020 Views
bryan_hong
Senior Contributor I

dear chillinwithscb 

thanks for your attention. I use below command.

PS X:\data\work\nxp\8MNANOLPD4-EVK\imx-android-14.0.0_2.2.0\android_build\out\target\product\evk_8mn> .\fastboot_imx_flashall.bat -f imx8mn -a -e -u trusty-dual -D .

 

and when I use uuu, I try to do with your comments.

 

Thanks,
Bryan

Tags (1)
0 Kudos
Reply
3,451 Views
bryan_hong
Senior Contributor I
bryan_hong_1-1694391805182.png

I have attached evk board I using

0 Kudos
Reply
3,411 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Your steps are correct, which system you are using?

0 Kudos
Reply
3,407 Views
bryan_hong
Senior Contributor I

it's android!!!

0 Kudos
Reply
3,399 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I mean Linux PC or Windows PC

0 Kudos
Reply
3,395 Views
bryan_hong
Senior Contributor I
I can use both all .
0 Kudos
Reply
3,385 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

I can flash with same steps.

There is two reasons about this error:

1. Your USB cable issue

2. EVK hardware issue.

0 Kudos
Reply
3,381 Views
bryan_hong
Senior Contributor I
I have 2or3 ea boards and will test them.
get back soon
0 Kudos
Reply
3,366 Views
bryan_hong
Senior Contributor I
I have 2ea evk 8m nano,

All did not work flashing emmc.

What should I do?
0 Kudos
Reply
3,316 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You can try other board, like 8mp, 8mm.

0 Kudos
Reply
3,497 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bryan_hong 

Please share the board photo.

Best Regards

Zhiming

0 Kudos
Reply