Flash configuration for NXP i.MX8M Mini Cortex-M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash configuration for NXP i.MX8M Mini Cortex-M4

3,436 Views
martindenion
Contributor II

I am currently working on the Cortex-M4 processor of the NXP i.MX8M Mini.
I am able to load the M4 binary from U-boot via DDR and TCM.
I would like now to program the M4 via a JTAG probe.
So I have created a project on SEGGER J-Flash and I can connect via the probe.
However, I don't know what configuration to enter to flash the program.

Probe: SEGGER 5.07.01 Flasher ARM
Flashing software : SEGGER J-Flash V7.50
OS : Windows 10
Development board : i.MX 8M Mini EVK

Labels (1)
0 Kudos
Reply
1 Reply

3,426 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

You may try as specified in the SDK documentation attached, chapter 5.1.3 Run an example application

Best regards,
Aldo.

0 Kudos
Reply