Connecting two image sensors to the i.MX 8M Nano EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connecting two image sensors to the i.MX 8M Nano EVK

510 Views
Ivan556
Contributor I

We need a quick solution for prototyping a dual-sensor system with the named EVK as the core. The sync requirements are really slight, so we'd like to avoid any aggregator ICs for now. What is of a question however, is the presence of only one MIPI-CSI clock line. Is this possible (say, by assigning a different input as the second sensor's CSI clock), or there is no way to get it done without an additional chip (either a MIPI aggregator, or a MIPI/parallel to USB bridge)?

0 Kudos
Reply
1 Reply

503 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ivan

 

I am afraid it is not possible to connect two sensors as i.MX8M Nano has one mipi-csi module.

As alternative one can consider for example usb camera.

 

Best regards
igor

0 Kudos
Reply