Firmware Compatible between iMX8M Nano & Mini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware Compatible between iMX8M Nano & Mini

Jump to solution
2,251 Views
milav_soni
Contributor III

 

Hello,

I want to confirm one thing in the form of compatibility.

Is imx8mnevk Build Yocto images and Test applications compatible with imx8mmevk?

are they both firmware compatible? can i use Bootloader, kernel and filesystem of imx8m nano for the  development of the imx8m mini?

Please Provide me your input for the same.

Thank You

 

 

0 Kudos
Reply
1 Solution
2,242 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello milav,

 

Yes, they are compatible from the bootloader and kernel, but you don´t have all the features as example for MX8MMini you have another cortex M4 and for MX8MNano you have the M7, now the feature of graphics you have in MX8MMini OpenGL 2.0 while in MX8MNano you have openGL 3.1 and openCL 1.2.

Regards

 

View solution in original post

2 Replies
2,243 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello milav,

 

Yes, they are compatible from the bootloader and kernel, but you don´t have all the features as example for MX8MMini you have another cortex M4 and for MX8MNano you have the M7, now the feature of graphics you have in MX8MMini OpenGL 2.0 while in MX8MNano you have openGL 3.1 and openCL 1.2.

Regards

 

2,233 Views
milav_soni
Contributor III

Hello, 

Thank You For your answer.

0 Kudos
Reply