Firmware Compatible between iMX8M Nano & Mini

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Firmware Compatible between iMX8M Nano & Mini

跳至解决方案
2,252 次查看
milav_soni
Contributor III

 

Hello,

I want to confirm one thing in the form of compatibility.

Is imx8mnevk Build Yocto images and Test applications compatible with imx8mmevk?

are they both firmware compatible? can i use Bootloader, kernel and filesystem of imx8m nano for the  development of the imx8m mini?

Please Provide me your input for the same.

Thank You

 

 

0 项奖励
回复
1 解答
2,243 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello milav,

 

Yes, they are compatible from the bootloader and kernel, but you don´t have all the features as example for MX8MMini you have another cortex M4 and for MX8MNano you have the M7, now the feature of graphics you have in MX8MMini OpenGL 2.0 while in MX8MNano you have openGL 3.1 and openCL 1.2.

Regards

 

在原帖中查看解决方案

2 回复数
2,244 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello milav,

 

Yes, they are compatible from the bootloader and kernel, but you don´t have all the features as example for MX8MMini you have another cortex M4 and for MX8MNano you have the M7, now the feature of graphics you have in MX8MMini OpenGL 2.0 while in MX8MNano you have openGL 3.1 and openCL 1.2.

Regards

 

2,234 次查看
milav_soni
Contributor III

Hello, 

Thank You For your answer.

0 项奖励
回复