Fingerprint property missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fingerprint property missing

ソリューションへジャンプ
2,674件の閲覧回数
michaelrobbelot
Contributor IV

Anyone,

I was wondering if anyone might know why ro.build.fingerprint would not show in an android build. I can clearly see that it is getting generated and is included in out/product/.../system/build.prop, but does not show up on the running build when you issue the getprop command or run the appropriate CTS test that looks for ro.build.fingerprint. Thanks.

Michael Robbeloth

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,304件の閲覧回数
michaelrobbelot
Contributor IV

I discovered that my fingerprint value was exceeding the maximum length of a property (defined to be PROPERTY_VALUE_MAX 92 in system/core/include/cutils/properties.h).

Michael Robbeloth

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,305件の閲覧回数
michaelrobbelot
Contributor IV

I discovered that my fingerprint value was exceeding the maximum length of a property (defined to be PROPERTY_VALUE_MAX 92 in system/core/include/cutils/properties.h).

Michael Robbeloth

0 件の賞賛
返信