Fingerprint property missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fingerprint property missing

Jump to solution
1,840 Views
michaelrobbelot
Contributor IV

Anyone,

I was wondering if anyone might know why ro.build.fingerprint would not show in an android build. I can clearly see that it is getting generated and is included in out/product/.../system/build.prop, but does not show up on the running build when you issue the getprop command or run the appropriate CTS test that looks for ro.build.fingerprint. Thanks.

Michael Robbeloth

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,470 Views
michaelrobbelot
Contributor IV

I discovered that my fingerprint value was exceeding the maximum length of a property (defined to be PROPERTY_VALUE_MAX 92 in system/core/include/cutils/properties.h).

Michael Robbeloth

View solution in original post

0 Kudos
Reply
1 Reply
1,471 Views
michaelrobbelot
Contributor IV

I discovered that my fingerprint value was exceeding the maximum length of a property (defined to be PROPERTY_VALUE_MAX 92 in system/core/include/cutils/properties.h).

Michael Robbeloth

0 Kudos
Reply