File transfer between imx28 and host PC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

File transfer between imx28 and host PC

1,623 次查看
alexaldridge
Contributor I

Hello mates!

I'm quite noob with the imx28 evaluation board. I've been able to flash a kernel to a SD card and boot from there. Also I've been able to log to the board using RS232 terminal.

I'd like to install java and transfer some files from my host PC to the board. Any help would be appreciated.

标记 (2)
0 项奖励
回复
3 回复数

1,511 次查看
b36401
NXP Employee
NXP Employee

You can use use z-modem protocol in the terminal you are using to connect the board.

First you need to connect the board and run "rz" utility. It will wait for the file to be sent.

Then you need to transfer the file from the terminal.

For example in minicom you need to press Ctrl+A and Z and then S for this option.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,511 次查看
alexaldridge
Contributor I

Thanks for the suggestion. If I do rz in my mx28 I get: "rz not found".

:smileysad:

0 项奖励
回复

1,511 次查看
Yuri
NXP Employee
NXP Employee

Hello,

You may try using WinSCP on Windows host.

Regards,

Yuri.

0 项奖励
回复