Fec rmii imx93

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fec rmii imx93

967 次查看
jsangwan
Contributor I
&fec {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec>;
phy-mode = "rmii";
phy-handle = <&ethphy2>;
fsl,magic-packet;
fsl,rmii_refclk_ext; // PHY provides 50MHz reference clock
enet_clk_sel = <&wakeupmix_gpr 0x2C>; // Required for RMII clock selection
status = "okay";

// PHY reset configuration
phy-reset-gpios = <&gpio2 25 GPIO_ACTIVE_LOW>;
phy-reset-duration = <10>;
phy-reset-post-delay = <10>;
 
mdio {
#address-cells = <1>;
#size-cells = <0>;
clock-frequency = <5000000>;

ethphy2: ethernet-phy@0 {
compatible = "ethernet-phy-ieee802.3-c22";
reg = <0>;
reset-gpios = <&gpio2 25 GPIO_ACTIVE_LOW>;
reset-assert-us = <10000>;
reset-deassert-us = <30000>;
max-speed = <100>; // RMII supports up to 100Mbps
};
};
};

these are my dts configrations i have a phy that generates clock 

in this configration eth0 pops up but only tx packets come up in ifconfig no rx packet 
 
pinctrl_fec: fecgrp {
fsl,pins = <
// MDIO interface
MX93_PAD_ENET2_MDC__ENET1_MDC 0x57e
MX93_PAD_ENET2_MDIO__ENET1_MDIO 0x57e
 
// RMII data pins
MX93_PAD_ENET2_RD0__ENET1_RGMII_RD0 0x57e
MX93_PAD_ENET2_RD1__ENET1_RGMII_RD1 0x57e
MX93_PAD_ENET2_RX_CTL__ENET1_RGMII_RX_CTL 0x57e
MX93_PAD_ENET2_TD0__ENET1_RGMII_TD0 0x57e
MX93_PAD_ENET2_TD1__ENET1_RGMII_TD1 0x57e
MX93_PAD_ENET2_TX_CTL__ENET1_RGMII_TX_CTL 0x57e
 
MX93_PAD_ENET2_TD2__ENET1_TX_CLK 0x4000057e
 
// PHY reset pin
MX93_PAD_GPIO_IO25__GPIO2_IO25 0x3fe
>;
};
0 项奖励
回复
1 回复

937 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

Please measure the TX_CLK pin with an oscilloscope to see if there is really a 50MHz square wave.

Your configuration is as follows:

//
phy-reset-duration = <10>;
phy-reset-post-delay = <10>;

//
reset-assert-us = <10000>;
reset-deassert-us = <30000>;


This is redundant, usually just the reset-gpios inside the mdio will suffice, it is recommended to keep only one reset control.



Best Regards,
Zhiming

0 项奖励
回复