Hi,
I verified the fastboot with a system.img (280MB) and confirmed it's working correctly (download and flash OK).
When I tried to use fastboot to flash the system.img (512MB), I saw two different errors:
1. FAILED (remote: data too large) on PC and send: FAILdata too large on iMX6
when I set
#define CONFIG_FASTBOOT_TRANSFER_BUF 0x2C000000
#define CONFIG_FASTBOOT_TRANSFER_BUF_SIZE 0x14000000 /* 320M byte */
I assumed it's because not enough transfer buffer and increased the size, but got #2 error below
2. FAILED (data transfer failure (Unknown error)), fastboot exits on PC and the iMX6 stuck on receiving data with 8~9 dots (.........)
When I set
#define CONFIG_FASTBOOT_TRANSFER_BUF 0x48000000
#define CONFIG_FASTBOOT_TRANSFER_BUF_SIZE 0x22000000 /* 320M byte */
Does anybody see the same failure before? Please help determine whether PC or iMX6 causes the problem. Thanks.
 
					
				
		
William
This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.
Thanks,
Yixing
Yiking,
I realize this is an old thread, but I would to reopen it. Are you aware of any patches to the fastboot source that will permit the uploading of data in chuncks to work around the limit discovered earlier in this thread. In particular, the userdata partition I work with is nearly 4.0 GB in size? Thank you.
Michael Robbeloth
Hi Jimmy,
Here is the partition definition in the mksdcard-android.sh.tar. The size of SYSTEM partition is 512MB.
#!/bin/sh
# partition size in MB
BOOTLOAD_RESERVE=8
BOOT_ROM_SIZE=8
SYSTEM_ROM_SIZE=512
DATA_SIZE=2048
CACHE_SIZE=512
RECOVERY_ROM_SIZE=8
VENDER_SIZE=8
MISC_SIZE=8
Is there a size limitation for fastboot to transfer?
 
					
				
		
William
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.
Thanks,
Yixing
 
					
				
		
 jimmychan
		
			jimmychan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		
So, have you try to change the size bigger?
 
					
				
		
 jimmychan
		
			jimmychan
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please check the 4.1.1 Storage Partitions in the Android BSP User Guide. Double check if your image is exceeded the size of the defined partition or not.