Change the debug console from ttymxc0 to ttyUSB0 for IMX6 Android LP5.0-GA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Change the debug console from ttymxc0 to ttyUSB0 for IMX6 Android LP5.0-GA

跳至解决方案
2,041 次查看
mayqueen
Contributor IV

Hello All:

KERNEL version: 3.10.53

As title, it works for yocto and ubuntu (just change the bootargs), but for Android 5.0, I only can disable the ttymxc0 (bootargs:115200 console=ttyUSB0,115200  rootwait androidboot.console=ttyUSB0 androidboot.hardware=freescale vmalloc=400M), but when I connect the USB cable, it's no any message....

Any  better and simple idea to implement this feature, I think maybe enable or modify something only in the kernel.

Thank you so much!

标签 (4)
标记 (3)
0 项奖励
回复
1 解答
1,524 次查看
mayqueen
Contributor IV

I solved it using busybox getty command!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,525 次查看
mayqueen
Contributor IV

I solved it using busybox getty command!

0 项奖励
回复
1,524 次查看
alejandrolozan1
NXP Employee
NXP Employee

H,

Would you be nice enough to share the command you used or the stpes for getty?

That would be very appreciated.

Best Regards,

Alejandro

0 项奖励
回复