Fastboot flashing not working on iMX8M Mini DDR4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fastboot flashing not working on iMX8M Mini DDR4

跳至解决方案
12,040 次查看
Hrithik
Contributor III

Hi NXP Team,

We are working on Android 11 on iMX8M Mini DDR4 board.

.
When we try to flash android images using fastboot, it gives following error:
FAILED (remote: device is locked.)

When we try fastboot OEM unlock command, it gives below error:

FAILED (remote: 'Unable to open fastboot HAL')
fastboot: error: Command failed

When we try fastboot flashing unlock:
FAILED (remote: unlock device failed.)

We tried both "adb reboot fastboot" as well as "adb reboot bootloader".
Fastboot device is detected after the command but not able to flash after that.

We got one log after UUU flashing - In boota get fastboot lock status error. Set lock status

Kindly help us in solving this issue.

Thanks.

标记 (2)
0 项奖励
回复
1 解答
11,948 次查看
Hrithik
Contributor III

Hi @Zhiming_Liu ,

 

Thanks for the reply.

But we had tried all these commands prior to posting it here.

We resolved the issue by enabling the "trusty" flag in the defconfig.

 

Regards,

Hrithik

在原帖中查看解决方案

0 项奖励
回复
3 回复数
12,021 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi 

Please try to enter uboot fastboot mode:

Qmiller_0-1650765252476.png

 

0 项奖励
回复
11,949 次查看
Hrithik
Contributor III

Hi @Zhiming_Liu ,

 

Thanks for the reply.

But we had tried all these commands prior to posting it here.

We resolved the issue by enabling the "trusty" flag in the defconfig.

 

Regards,

Hrithik

0 项奖励
回复
9,622 次查看
venu_mos
Contributor II

Hi,

in which def config file i need to add trusty flag, can you share the path ?

Thanks.

0 项奖励
回复