Fast-mode Plus on i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fast-mode Plus on i.MX6

ソリューションへジャンプ
2,084件の閲覧回数
inmaku
Contributor III

Hi,

The current I2C specification lists 3 modes of Operation: Standard mode, fast-mode and fast-mode plus. The latter one goes up to 1MHz clock frequency. In the iMX6 reference Manual, I can only find, that the Standard and fast modes are supported. Is that correct or can the i.MX6 be switched into the fast-mode plus?

Thanks,

Ingo

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,813件の閲覧回数
Yuri
NXP Employee
NXP Employee

The i.MX6 I2C supports standard and fast-mode, but does NOT support the fast-mode plus.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,814件の閲覧回数
Yuri
NXP Employee
NXP Employee

The i.MX6 I2C supports standard and fast-mode, but does NOT support the fast-mode plus.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信