Fast-mode Plus on i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fast-mode Plus on i.MX6

Jump to solution
810 Views
inmaku
Contributor III

Hi,

The current I2C specification lists 3 modes of Operation: Standard mode, fast-mode and fast-mode plus. The latter one goes up to 1MHz clock frequency. In the iMX6 reference Manual, I can only find, that the Standard and fast modes are supported. Is that correct or can the i.MX6 be switched into the fast-mode plus?

Thanks,

Ingo

Labels (1)
Tags (2)
0 Kudos
1 Solution
539 Views
Yuri
NXP Employee
NXP Employee

The i.MX6 I2C supports standard and fast-mode, but does NOT support the fast-mode plus.


Have a great day,
Yuri
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
540 Views
Yuri
NXP Employee
NXP Employee

The i.MX6 I2C supports standard and fast-mode, but does NOT support the fast-mode plus.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos