Failure compiling busybox with PAM support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure compiling busybox with PAM support

1,890 Views
josévicentesana
Contributor I

I am using L2.6.31_09.12.01

I have selected support for PAM in busybox package.

The result of the compilation of busybox package is like this:

pam_appl.h  No such file or directory

pam_misc.h: No such file or directory

and many other error.

I think i need to add another options or packages but i don´t know what options or packages to add

Has anybody know what to do in that situation?

Labels (1)
0 Kudos
Reply
1 Reply

1,548 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Vicente,

Are you using LTIB for this compilation? what version of BSP are you using?  Check the makefile of the BusyBox ( PAM)  in order to see the dependencies required or in the readme file what requirements of the Kernel or options need to be setup.

saludos

Jaime

0 Kudos
Reply