Failure compiling busybox with PAM support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failure compiling busybox with PAM support

2,375件の閲覧回数
josévicentesana
Contributor I

I am using L2.6.31_09.12.01

I have selected support for PAM in busybox package.

The result of the compilation of busybox package is like this:

pam_appl.h  No such file or directory

pam_misc.h: No such file or directory

and many other error.

I think i need to add another options or packages but i don´t know what options or packages to add

Has anybody know what to do in that situation?

ラベル(1)
0 件の賞賛
返信
1 返信

2,033件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Vicente,

Are you using LTIB for this compilation? what version of BSP are you using?  Check the makefile of the BusyBox ( PAM)  in order to see the dependencies required or in the readme file what requirements of the Kernel or options need to be setup.

saludos

Jaime

0 件の賞賛
返信