Hi,
I've designed new board using i.MX6 Q CPU and reference has been taken from Sabrelite board.
There is only differences in DDR3 interface like Data Bus mapping. I've used straight D0-D64 between i.MX6Q and DDR3 (Micron) Chip MT41J128M16HA-15E.
I am using OCDemaon USB Wiggler hardware and OCD Commander (Software) for JTAG programming in Windows 7.
I am getting error below:
"Memory Write Error : 0x27800000 - 27801000
HALT"
I've tried DDR3 stress test at 400MHz and it was going till loop 9. Then i just stopped it.
I am not sure where the exact problem is.
It seems DDR3 is working but not sure.
Am i missing some hardware setting which should be done for fresh board?
Please let me know your views.