Failing Sabrelite *.elf file download in Custom Board using JTAG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failing Sabrelite *.elf file download in Custom Board using JTAG

1,616 次查看
anujsinghvi
Contributor II

Hi,

I've designed new board using i.MX6 Q CPU and reference has been taken from Sabrelite board.

There is only differences in DDR3 interface like Data Bus mapping.  I've used straight D0-D64 between i.MX6Q and DDR3 (Micron) Chip  MT41J128M16HA-15E.

I am using OCDemaon USB Wiggler hardware and OCD Commander (Software) for JTAG programming in Windows 7.   

I am getting error below:

"Memory Write Error : 0x27800000 - 27801000

HALT"

I've tried DDR3 stress test at 400MHz and it was going till loop 9.  Then i just stopped it.

I am not sure where the exact problem is. 

It seems DDR3 is working but not sure.

Am i missing some hardware setting which should be done for fresh board?

Please let me know your views.

标签 (1)
0 项奖励
回复
3 回复数

1,499 次查看
YixingKong
Senior Contributor IV

Anuj

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复

1,499 次查看
YixingKong
Senior Contributor IV

Anuj

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复

1,499 次查看
YixingKong
Senior Contributor IV

Anuj

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复