Failed to play mp4 clip using gstreamer using waylandsink

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Failed to play mp4 clip using gstreamer using waylandsink

5,552 次查看
jehunkim
Contributor I

I'm trying to play an mp4 video back using gstreamer on the wayland backend

but I'm having trouble with playing mp4 video clip.

My environment is like this.

board : i.mx6q sabreauto

branch : imx-3.14.38-6QP_ga

image : bitbake fsl-image-gui

graphic backend : wayland backend

command

$export GSTL=gst-launch-1.0

$export PLAYBIN=playbin

$export GPLAY=gplay-1.0

$export GSTINSPECT=gst-inspect-1.0

$GSTL -v filesrc location=clip.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! waylandsink

The error message is like this.

[INFO]  Product Info: i.MX6Q/D/S

====== VPUDEC: 4.0.7 build on Mar  4 2016 19:06:40. ======

    wrapper: 1.0.61 (VPUWRAPPER_ARM_LINUX Build on Feb 18 2016 11:53:25)

    vpulib: 5.4.31

    firmware: 3.1.1.46070

Pipeline is PREROLLING ...

Got context from element 'waylandsink0': GstWaylandDisplayHandleContextType=context, handle=(gpointer)NULL;

====== AIUR: 4.0.7 build on Mar  4 2016 19:06:32. ======

    Core: MPEG4PARSER_06.09.16  build on Jun 29 2015 05:17:33

file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2

------------------------

    Track 00 [video_0] Enabled

    Duration: 0:00:30.000000000

    Language: und

    Mime:

    video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1920, height=(int)720, framerate=(fraction)30/1, codec_data=(buffer)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20

------------------------

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = "video/x-h264\,\ parsed\=\(boolean\)true\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)avc\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ framerate\=\(fraction\)30/1\,\ codec_data\=\(buffer\)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20"

/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:sink: caps = "video/x-h264\,\ parsed\=\(boolean\)true\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)avc\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ framerate\=\(fraction\)30/1\,\ codec_data\=\(buffer\)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20"

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = "video/x-h264\,\ parsed\=\(boolean\)true\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)avc\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ framerate\=\(fraction\)30/1\,\ codec_data\=\(buffer\)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20"

[INFO]  bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)NV12\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ interlace-mode\=\(string\)progressive\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)30/1"

ERROR: from element /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0: GStreamer encountered a general stream error.

Additional debug info:

/home/lbox/idc/bsp/build/tmp/work/imx6qsabreauto-poky-linux-gnueabi/gst1.0-fsl-plugin/4.0.7-r0/gst1.0-fsl-plugins-4.0.7/plugins/aiurdemux/aiurdemux.c(1007): aiurdemux_pull_task (): /GstPipeline:pipeline0/GstAiurDemux:aiurdemux0:

streaming stopped, reason not-negotiated, state 3

ERROR: pipeline doesn't want to preroll.

Setting pipeline to NULL ...

/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:src: caps = "NULL"

/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:sink: caps = "NULL"

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = "NULL"

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = "NULL"

/GstPipeline:pipeline0/GstAiurDemux:aiurdemux0.GstPad:video_0: caps = "NULL"

Freeing pipeline ...

but if i run next command

$GSTL -v filesrc location=clip.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! overlaysink

There's no problem. It's working. But the video clip is playing on the fbdev backend not the wayland.

Can someone please tell me what I might be doing wrong?

Thanks!

0 项奖励
回复
4 回复数

3,023 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Have you tried imxv4l2sink?

Luis

0 项奖励
回复

3,023 次查看
jehunkim
Contributor I

I tryed imxv4l2sink.

But It's also playing on the fb backend(full screen) not wayland backend.

The difference of imxv4l2sink and overlaysink is the scaling of video clip.

The video is playing with same size of the video clip(1920x720) by overlaysink.

Using imxv4l2sink, the video is stretched to the full screen(1920x1080).

$GSTL -v filesrc location=clip.mp4 typefind=true ! video/quicktime ! aiurdemux ! queue max-size-time=0 ! vpudec ! imxv4l2sink

====== IMXV4L2SINK: 4.0.7 build on Mar  4 2016 19:06:36. ======

Setting pipeline to PAUSED ...

display(/dev/fb0) resolution is (1920x1080).

[INFO] Product Info: i.MX6Q/D/S

====== VPUDEC: 4.0.7 build on Mar  4 2016 19:06:40. ======

  wrapper: 1.0.61 (VPUWRAPPER_ARM_LINUX Build on Feb 18 2016 11:53:25)

  vpulib: 5.4.31

  firmware: 3.1.1.46070

Pipeline is PREROLLING ...

====== AIUR: 4.0.7 build on Mar  4 2016 19:06:32. ======

  Core: MPEG4PARSER_06.09.16  build on Jun 29 2015 05:17:33

file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2

------------------------

    Track 00 [video_0] Enabled

  Duration: 0:00:30.000000000

  Language: und

    Mime:

  video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)1920, height=(int)720, framerate=(fraction)30/1, codec_data=(buffer)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20

------------------------

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:src: caps = "video/x-h264\,\ parsed\=\(boolean\)true\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)avc\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ framerate\=\(fraction\)30/1\,\ codec_data\=\(buffer\)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20"

/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:sink: caps = "video/x-h264\,\ parsed\=\(boolean\)true\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)avc\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ framerate\=\(fraction\)30/1\,\ codec_data\=\(buffer\)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20"

/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = "video/x-h264\,\ parsed\=\(boolean\)true\,\ alignment\=\(string\)au\,\ stream-format\=\(string\)avc\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ framerate\=\(fraction\)30/1\,\ codec_data\=\(buffer\)0142c00dffe100176742c00df403c02dd80880000003008000001e078a155001000568ce010f20"

[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0

/GstPipeline:pipeline0/GstVpuDec:vpudec0.GstPad:src: caps = "video/x-raw\,\ format\=\(string\)NV12\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ interlace-mode\=\(string\)progressive\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)30/1"

/GstPipeline:pipeline0/GstImxV4l2Sink:imxv4l2sink0.GstPad:sink: caps = "video/x-raw\,\ format\=\(string\)NV12\,\ width\=\(int\)1920\,\ height\=\(int\)720\,\ pixel-aspect-ratio\=\(fraction\)1/1\,\ interlace-mode\=\(string\)progressive\,\ colorimetry\=\(string\)bt709\,\ framerate\=\(fraction\)30/1"

v4l2sink need allocate 9 buffers.

Pipeline is PREROLLED ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

Got EOS from element "pipeline0".

Execution ended after 0:00:30.002519671

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

Setting pipeline to NULL ...

Total showed frames (816), playing for (0:00:30.004343004), fps (27.196).

Freeing pipeline ...

0 项奖励
回复

3,023 次查看
joanxie
NXP TechSupport
NXP TechSupport

when you use the command "gst-inspect waylandsink", what do you find? have you installed this sink already?

0 项奖励
回复

3,023 次查看
jehunkim
Contributor I

Yes. I installed waylandsink and the result is as below

root@imx6qsabreauto:~# gst-inspect-1.0 waylandsink

Factory Details:

  Rank                    marginal (64)

  Long-name                wayland video sink

  Klass                    Sink/Video

  Description              Output to wayland surface

  Author                  Sreerenj Balachandran <sreerenj.balachandran@intel.com>, George Kiagiadakis <george.kiagiadakis@collabora.com>

Plugin Details:

  Name                    waylandsink

  Description              Wayland Video Sink

  Filename                /usr/lib/gstreamer-1.0/libgstwaylandsink.so

  Version                  1.4.5

  License                  LGPL

  Source module            gst-plugins-bad

  Source release date      2014-12-18

  Binary package          GStreamer Bad Plug-ins source release

  Origin URL              Unknown package origin

GObject

+----GInitiallyUnowned

      +----GstObject

            +----GstElement

                  +----GstBaseSink

                        +----GstVideoSink

                              +----GstWaylandSink

Implemented Interfaces:

  GstVideoOverlay

  GstWaylandVideo

Pad Templates:

  SINK template: 'sink'

    Availability: Always

    Capabilities:

      video/x-raw

                format: { BGRx, BGRA, RGBx, xBGR, xRGB, RGBA, ABGR, ARGB, RGB, BGR, RGB16, BGR16, YUY2, YVYU, UYVY, AYUV, NV12, NV21, NV16, YUV9, YVU9, Y41B, I420, YV12, Y42B, v308 }

                  width: [ 1, 2147483647 ]

                height: [ 1, 2147483647 ]

              framerate: [ 0/1, 2147483647/1 ]

Element Flags:

  no flags set

Element Implementation:

  Has change_state() function: gst_wayland_sink_change_state

Element has no clocking capabilities.

Element has no URI handling capabilities.

Pads:

  SINK: 'sink'

    Implementation:

      Has chainfunc(): gst_base_sink_chain

      Has custom eventfunc(): gst_base_sink_event

      Has custom queryfunc(): gst_base_sink_sink_query

      Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default

    Pad Template: 'sink'

Element Properties:

  name                : The name of the object

                        flags: readable, writable

                        String. Default: "waylandsink0"

  parent              : The parent of the object

                        flags: readable, writable

                        Object of type "GstObject"

  sync                : Sync on the clock

                        flags: readable, writable

                        Boolean. Default: true

  max-lateness        : Maximum number of nanoseconds that a buffer can be late before it is dropped (-1 unlimited)

                        flags: readable, writable

                        Integer64. Range: -1 - 9223372036854775807 Default: 20000000

  qos                : Generate Quality-of-Service events upstream

                        flags: readable, writable

                        Boolean. Default: true

  async              : Go asynchronously to PAUSED

                        flags: readable, writable

                        Boolean. Default: true

  ts-offset          : Timestamp offset in nanoseconds

                        flags: readable, writable

                        Integer64. Range: -9223372036854775808 - 9223372036854775807 Default: 0

  enable-last-sample  : Enable the last-sample property

                        flags: readable, writable

                        Boolean. Default: true

  last-sample        : The last sample received in the sink

                        flags: readable

                        Boxed pointer of type "GstSample"

  blocksize          : Size in bytes to pull per buffer (0 = default)

                        flags: readable, writable

                        Unsigned Integer. Range: 0 - 4294967295 Default: 4096

  render-delay        : Additional render delay of the sink in nanoseconds

                        flags: readable, writable

                        Unsigned Integer64. Range: 0 - 18446744073709551615 Default: 0

  throttle-time      : The time to keep between rendered buffers (0 = disabled)

                        flags: readable, writable

                        Unsigned Integer64. Range: 0 - 18446744073709551615 Default: 0

  max-bitrate        : The maximum bits per second to render (0 = disabled)

                        flags: readable, writable

                        Unsigned Integer64. Range: 0 - 18446744073709551615 Default: 0

  show-preroll-frame  : Whether to render video frames during preroll

                        flags: readable, writable

                        Boolean. Default: true

  display            : Wayland display name to connect to, if not supplied via the GstContext

                        flags: readable, writable

                        String. Default: null

0 项奖励
回复