Facing U-Boot Error after flashing the Hardknott Image into Nitrogrn8m

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Facing U-Boot Error after flashing the Hardknott Image into Nitrogrn8m

1,499 次查看
rohithch
Contributor I

Device: Nitrogen8M
OS: Hardknott (Yocto)

 

U-Boot SPL 2020.10-53235-g9580b06f2c (Apr 06 2022 - 13:42:57 -0700)            

Setting voltages                                                               

config to do 3200 1d training.                                                 

config to do 667 1d training.                                                  

config to do 3200 2d training.                                                 

Normal Boot                                                                    

Trying to boot from MMC1                                                       

                                                                               

                                                                               

U-Boot 2020.10-53235-g9580b06f2c (Apr 06 2022 - 13:42:57 -0700), Build: jenkins9

                                                                               

CPU:   i.MX8MQ rev2.0 at 1000 MHz                                              

Reset cause: POR                                                               

Model: Boundary Devices i.MX8MQ Nitrogen8M_som                                 

Board: nitrogen8m_som                                                          

       Watchdog enabled                                                        

DRAM:  4 GiB                                                                   

MMC:   FSL_SDHC: 0                                                             

Loading Environment from MMC...                                                

OK                                                                             

auto-detected panel m101nwwb                                                   

Display: mipi:m101nwwb (1280x800)                                              

[*]-Video Link 0 (1280 x 800)                                                  

        [0] lcdif@30320000, video                                              

        [1] mipi-dsi-bridge, video_bridge                                      

        [2] panel@0, panel                                                     

In:    serial                                                                  

Out:   serial                                                                  

Err:   serial                                                                  

                                                                               

 BuildInfo:                                                                    

  - ATF adf9668                                                                

                                                                               

Net:   AR8035 at 4                                                             

FEC [PRIME], usb_ether                                                         

Hit any key to stop autoboot:  0                                               

switch to partitions #0, OK                                                    

mmc0(part 0) is current device                                                 

Saving Environment to MMC... Writing to MMC(0)... OK                           

1                                                                              

Scanning mmc 0:1...                                                            

Found U-Boot script /upgrade.scr                                               

Invalid FAT entry                                                              

** Unable to read file /upgrade.scr **                                         

Failed to load '/upgrade.scr'                                                  

## Executing script at 40480000                                                

Bad data crc                                                                   

script exited: continuing...                                                   

load - load binary file from a filesystem                                      

                                                                               

Usage:                                                                         

load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]]            

    - Load binary file 'filename' from partition 'part' on device              

       type 'interface' instance 'dev' to address 'addr' in memory.            

      'bytes' gives the size to load in bytes.                                 

      If 'bytes' is 0 or omitted, the file is read until the end.              

      'pos' gives the file byte position to start reading from.                

      If 'pos' is 0 or omitted, the file is read from the start.               

=>

0 项奖励
回复
3 回复数

1,467 次查看
rohithch
Contributor I

No, I tried to flash the image given by the Boundary devices it caused a " Panic Kernel Error".

we downloaded Hardknott Image from https://boundarydevices.com/yocto-hardknott-release-for-i-mx8-platforms/

 

kernelpanic.png

 

0 项奖励
回复

1,463 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

You should post this issue in Boundary devices community.

The BSP provided by Boundary devices is different from NXP.

1,473 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Can you flash images provided by Nitrogrn8m?

0 项奖励
回复