Device: Nitrogen8M
OS: Hardknott (Yocto)
U-Boot SPL 2020.10-53235-g9580b06f2c (Apr 06 2022 - 13:42:57 -0700)
Setting voltages
config to do 3200 1d training.
config to do 667 1d training.
config to do 3200 2d training.
Normal Boot
Trying to boot from MMC1
U-Boot 2020.10-53235-g9580b06f2c (Apr 06 2022 - 13:42:57 -0700), Build: jenkins9
CPU: i.MX8MQ rev2.0 at 1000 MHz
Reset cause: POR
Model: Boundary Devices i.MX8MQ Nitrogen8M_som
Board: nitrogen8m_som
Watchdog enabled
DRAM: 4 GiB
MMC: FSL_SDHC: 0
Loading Environment from MMC...
OK
auto-detected panel m101nwwb
Display: mipi:m101nwwb (1280x800)
[*]-Video Link 0 (1280 x 800)
[0] lcdif@30320000, video
[1] mipi-dsi-bridge, video_bridge
[2] panel@0, panel
In: serial
Out: serial
Err: serial
BuildInfo:
- ATF adf9668
Net: AR8035 at 4
FEC [PRIME], usb_ether
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0(part 0) is current device
Saving Environment to MMC... Writing to MMC(0)... OK
1
Scanning mmc 0:1...
Found U-Boot script /upgrade.scr
Invalid FAT entry
** Unable to read file /upgrade.scr **
Failed to load '/upgrade.scr'
## Executing script at 40480000
Bad data crc
script exited: continuing...
load - load binary file from a filesystem
Usage:
load <interface> [<dev[:part]> [<addr> [<filename> [bytes [pos]]]]]
- Load binary file 'filename' from partition 'part' on device
type 'interface' instance 'dev' to address 'addr' in memory.
'bytes' gives the size to load in bytes.
If 'bytes' is 0 or omitted, the file is read until the end.
'pos' gives the file byte position to start reading from.
If 'pos' is 0 or omitted, the file is read from the start.
=>
No, I tried to flash the image given by the Boundary devices it caused a " Panic Kernel Error".
we downloaded Hardknott Image from https://boundarydevices.com/yocto-hardknott-release-for-i-mx8-platforms/
Can you flash images provided by Nitrogrn8m?