FTP setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTP setup

2,222件の閲覧回数
goodwell
Contributor I

Hi,

I made an image for a sabrelite board using yocto; fsl-image-test. The image boots and runs fine, but I cannot transfer files through FileZilla ftp or sftp. I can connect to the target through ssh but when I try to use FileZilla the connection is rejected. What do I need enabled or installed on the target to allow for file transfers?

Thanks!

0 件の賞賛
返信
2 返答(返信)

2,000件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Scott,

So you are running ubuntu already and you are using filezilla from your pc to connect to the board?

0 件の賞賛
返信

2,000件の閲覧回数
goodwell
Contributor I

Hi, thanks for the reply,

I do have this working now, I had vsftpd installed on the target and it

needed to be configured.

I enabled anonymous logins for testing and was able to establish a

connection after that.

Thanks again

0 件の賞賛
返信