FT5x06 Touch screen issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FT5x06 Touch screen issue.

2,386 Views
hrushinale
Contributor III

Hello all,

I am using a custom board running on i.MX6 solo. On our board I tried to bring up the FT5x06 capacitive touchscreen for that I used ft5x06_ts.c driver from boundary devices .

Now, the touch screen is working fine if I am loading the driver as a MOdule but its not working if I load the driver in the kernel itself(After touching the screen the cursot will move to one corner and will not move from there.)

I am unable to make the touch work without loading the drivers manually.

I am using kernel version 3.14.28 and  yocto rootfs.

Kindly help regarding this issue.

Best Regards,

Hrushi

Tags (2)
0 Kudos
Reply
3 Replies

2,171 Views
aravinthkumarja
Senior Contributor II

Hi,

Can you attach the driver file and Kconfig and touch initialization add dts file.

Regards,

Aravinth

0 Kudos
Reply

2,171 Views
hrushinale
Contributor III

Thanks aravinthkumar jayaprakasam for reply.

Its working now after doing some changes in Rootfs.

Thanks & Regards,

Hrushi

0 Kudos
Reply

2,171 Views
aravinthkumarja
Senior Contributor II

Hi Hrushi,

Thanks, All the best.

Regards,

Aravinth

0 Kudos
Reply